DRV.CPUPERCENT
Description
DRV.CPUPERCENT returns a percentage representing the execution time of the 16kHz loop versus the total 16kHz period (62.5us).
This keyword can be used to approximate the load on the drive’s processor.
-
- If this value exceeds 75%, F3008 will occur.
Parameter Value | Drive Action |
---|---|
0 | Disable Amplifier |
1 | Ignore. Fault will not be reported. |
General Information
Type | Read Only |
Units | Percent |
Range | N/A |
Default Value | N/A |
Data Type | Float |
Stored in Non-Volatile Memory |
No |
Variants Supported
AKD2G
Fieldbus Information
Command |
Index |
SubIndex |
Data Type |
Units |
Float Scale |
Access |
|
---|---|---|---|---|---|---|---|
DRV.CPUPERCENT |
3000h |
0ah |
Unsigned16 |
- |
- |
Read only |
Yes |
Name |
ID |
Hex |
Data Type |
Access |
Units |
---|---|---|---|---|---|
DRV.CPUPERCENT |
2024 |
7E8 |
Unsigned16 |
Read Only |
- |
Parameter |
PNU |
Data Type |
Access |
Units |
---|---|---|---|---|
DRV.CPUPERCENT |
2024 |
Float |
Read Only |
- |